Markup Support for Sessions

In the Editor XI plugin for Solution Center, you can view markups that are assigned to sessions. To learn more about Markups, refer to the Markup and Markup Types topic.
  1. Select a session in the Session Manager tab.
  2. Click the Markups tab to display a list of markups, along with who they are assigned to, and when they were submitted.
    Markups associated with a session

    There are no available tools in the Editor XI Solution Center plugin to alter the assignment of the markups.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.