Session Manager Tab

Session Manager allows you to create and edit sessions that follow a specific version structure and user roles that have been configured. Session Manager creates an edit session in which an editor can make changes. After the changes are complete, the user sends the session through an approval process. Each session has its own associated version.

Take it for a drive!

(That link opens/switches to the Solution Center app and accesses the Session Manager tab.)

Additional workflows are supported as a configuration in Azure. A session (and its associated version) may travel through the process several times before receiving approval and being posted to the geodatabase. The following diagram represents an example workflow.


A flow chart illustrating a sample Session Manager workflow

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.