2505_LSS900100_eConfigure_KNX_SW_03.0

Remote Connection Using VPN (Secure)

If you want to connect remotely to a KNX IP interface via the Internet, we recommend using a VPN connection, as this is a secure connection. Connect the KNX IP interface via VPN as follows:

  1. Connect your computer to a VPN.

  2. Go to the Upload tab in eConfigure and click Select Interface.  

  3. eConfigure/ETS cannot search for KNX IP interface through the VPN connection, so you have to add the interface manually: Click Add interface and fill in the Add interface form.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?