2505_LSS900100_eConfigure_KNX_SW_03.0

eConfigure Expert Installation

Install the eConfigure Expert software as follows:

  1. Go to my.knx.org > purchase eConfigure Expert > download it to your local storage.

  2. Launch the ETS software on your computer.

  3. ETS6: Go to Settings click Install app > select the installation file from your local storage > click Open.

    NOTE: In ETS5, click Apps on the right side of the bottom bar > click the plus sign to select the installer file from your local storage.

  4. After the installation is complete, open the ETS software again, open an existing project or create a new one.

  5. ETS6: In your project, go to Panels > All panels > Schneider Electric > click eConfigure Expert to launch it.

    NOTE: In ETS5, click Apps > click eConfigure Expert.

eConfigure Expert will launch as a new window in ETS and you can start to use it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?