2505_LSS900100_eConfigure_KNX_SW_03.0

Password Change

A password change is required if it does not meet the security requirements.

Password complexity requirements:

  • The length between 8 – 32 characters

  • At least one uppercase letter

  • At least one lowercase letter

  • At least one digit (0 – 9)

  • European languages letters (A – Z with diacritics, sharp S, Greek and Cyrillic characters)

The admin password will be changed on the controller during the next upload.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?