DOCA0191EN–05

Factory Settings

The overload relays are delivered with the factory settings as follows:

  • Thermal overload protection: enabled.

  • Ir/FLA threshold: Ir/FLA minimum value.

  • Reset mode: Manual.

  • Trip class: 10E.

  • Phase loss protection: enabled.

  • Phase imbalance protection: enabled.

  • Ground-fault protection: enabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.