DOCA0191EN–05

Precautions

Read and understand the following precautions before performing any procedures in this guide.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462,NOM 029-STPS or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on this equipment.
  • Use only the specified voltage when operating this equipment and any associated products.
  • Power line circuits must be wired and protected in compliance with local and national regulatory requirements.
  • Beware of potential hazards, and carefully inspect the work area for tools and objects that may have been left inside the equipment.
Failure to follow these instructions will result in death or serious injury.

Intended Use

The products described in this guide are low voltage switchgears intended for industrial use within industrial or commercial applications.

The product may only be used in compliance with all applicable safety regulations and directives, the specified requirements, and the technical data.

Before using the product, you must perform a hazard analysis and risk assessment of the planned application. Based on the results, appropriate safety related measures must be implemented.

Since the product is used as a component of a machine or process, you must ensure the safety of persons by means of the overall system design.

Operate the product only with the specified cables and accessories. Use only genuine accessories and spare parts. Any use other than the use explicitly permitted is prohibited and can result in unanticipated hazards.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.