DOCA0191EN–05

Control Module Removal

The control module can be replaced without power disconnection.

Before replacing the control module on a contactor:

  • Remove the plate on the side of the control module, if present

  • Remove all auxiliary contact modules.

Perform the following procedure to remove the control module:

  1. Unscrew the control terminal blocks.

  2. Remove the control terminal blocks.

  3. Open the flip cover under the control module.

  4. Push on the screws fixing the control module on the contactor with a screwdriver.

  5. Turn the screws 90° anti-clockwise to unlock the control module.

  6. Remove the control module from the contactor.

  7. Recycle the control module.

    NOTE: Clean the accessible parts of the contactor and visually check the overall condition of the contactor.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.