Mounting Star-Delta Contactors on Plate
Perform the following procedure to mount the star-delta contactors on the plate.
-
Drill 12 holes in the plate, with respect of the dimensions given.
-
LC1G205-475C - Maximum hole diameter: 6 mm
-
LC1G620C - Maximum hole diameter: 9 mm
NOTE: To ease the mounting, drilling stencils JYT1902701 can be downloaded from the www.se.com website.Star-delta starter with three contactors of the same size:Star-delta starter with LC1G300-475C line and delta contactors and LC1G205-245C star contactor. Star-delta starter with LC1G620C line and delta contactors and LC1G300-475C star contactor.Contactor
G
J
X
LC1G205-245C
35 mm
166 mm
92,7 mm
LC1G300-475C
45 mm
187 mm
115 mm
LC1G620C
70 mm
242 mm
160 mm
-
-
Remove the plastic part on the side of the star and delta contactors, where the mechanical interlock will be installed.
-
Discard the plastic part into the bin.
-
Insert the metal slides on the holes of the star and delta contactors.
-
Mount each contactor on the plate. Consult the relevant instructions:
-
For mounting LC1G205-245C contactors, see Mounting LC1G205-245C Contactors on Plate
-
For mounting LC1G300-620C contactors, see Mounting LC1G300-620C Contactors on Plate
-
-
Assemble the mechanical interlock LA9G970 between star and delta contactors of the same size according to the size of the contactors.
NOTE: The mechanical interlock LA9G971 and LA9G972 between star and delta contactors of different sizes do not need to be adapted. -
Insert the mechanical interlock between the star and delta contactors on the metal slides.
-
Tighten the two screws at the right torque to lock the interlock.