DOCA0191EN–05

Power Connection with Reverser Connection Kits

Overview

Reverser connection kits can be used for the power connection of a 3-pole two-contactor reverser. If using the connection kits, the two contactors must be fitted with a cable memory or must be without cable memory. The power connection can be done upstream and downstream of the contactors.

Reverser connection kits are made of two identical coupling bars.

The table below provides the list of the reverser connection kits:

Contactor

Reverser connection kits

LC1G205-245C

LA9G3760

 

LC1G300-475C

LA9G3761

 

LC1G620C

LA9G3762

 

Dimensions

Commercial reference

W0

W1

H0

D0

D1

P

LA9G3760

215.7 mm

232.6 mm

31.5 mm

23.6 mm

68.5 mm

20 mm

LA9G3761

280 mm

298 mm

38 mm

79 mm

81 mm

20 mm

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.