DOCA0191EN–05

Installation of the Power Connection Accessories

This section describes the installation procedure of straight terminal extensions on the power terminals. The installation procedure is same for all other power connection accessories.
  1. Place the terminal extension on the power terminals.
  2. Insert the screw and washer through the hole at the top of the terminal extension.
  3. Tighten the screws at the right torque.
    Contactor

    Type of screws

    Torque

    LC1G205-245C

    Allen key

    18±1.8 N•m

    LC1G300-475C

    Inner hexagon

    35±3.5 N•m

    LC1G620C

    Inner hexagon

    58±5.8 N•m

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?