DOCA0191EN–05

Contactor Customization

Overview

Cable memory connection blocks enable contactor replacement without disconnection of the power connections.

Cable memory connection blocks can be installed as an option on 3-pole contactors.

Description

Compatible with contactors

Cable memory reference

Cable memory for 3-pole contactors - for holding cables in place when replacing contactor

LC1G205–245C

LA9G3101

LC1G300–475C

LA9G3102

LC1G620C

LA9G3103

This section describes the cable memory connection blocks installation on the contactor .

Cable Memory Connection Blocks Installation on Contactor

  1. Place the screwdriver on the contactor power terminals to remove the snap-in nut.

  2. Twist the screwdriver clockwise.

  3. Pull the snap-in nut outwards to remove it.

    NOTE: Remove all the six nuts in similar way. Keep the lock nuts aside for further use.
  4. Place the cable memory connection blocks on the contactor power terminals.

  5. Push inwards to lock it automatically with a click.

  6. Place the lock nut back on the power terminals of the cable memory.

  7. Tighten the screws at the right torque.

Contactor

Torque

Tool

Screws

LC1G205–245C

18±1.8 N•m

Allen key

M8

LC1G300–475C

35±3.5 N•m

Inner hexagon

M10

LC1G620C

58±5.8 N•m

Inner hexagon

M12

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?