DOCA0191EN–05

Go2SE Landing Page

Presentation

When the QR code on the front face of a TeSys Giga series device is scanned with a smartphone having a QR code reader and connected to the internet, the Go2SE landing page is displayed.

The landing page displays information about the device and a list of menus.

Landing Page Description

The landing page is accessible from Android and iOS smartphones. It displays the same list of menus with slight differences in presentation.

The following example shows the landing page displayed on an android smartphone:

A Commercial reference of TeSys Giga series device

B Type of TeSys Giga series device

C Landing page menus. See the following menu descriptions for details.

D Downloadable applications

Characteristics

Selecting this menu gives access to the product datasheet with detailed information about the TeSys Giga series device.

Documentation

Selecting this menu gives access to the technical documentation related to the product.

用千里眼管理和维护您的资产

Selecting this application gives access to the 千里眼 mobile application that can be downloaded on Android and iOS smartphones. For smartphone compatibility, check on your application store.

千里眼 optimizes operations and maintenance, helping to ensure business continuity, and provides insights to service providers or facility managers.

千里眼 is a real-time collaborative technology available on mobile devices and PCs that enables managers and maintenance personnel to be connected with facilities and equipment. Information exchange between users is simple and fast.

The QR code on TeSys Giga series device enables managers and maintenance personnel to access the following automatic downloads:

  • TeSys Giga series device identifier.

  • Technical documentation.

  • The maintenance plan for the TeSys Giga series device.

千里眼 enables managers and maintenance personnel to access the maintenance plan for TeSys Giga series devices.

千里眼 helps maintenance personnel to diagnose issues remotely and manage maintenance efficiently by:

  • Providing relevant information on critical assets.

  • Sending immediate state of the equipment and detailed information helping for diagnostics.

mySchneider App

Selecting this application gives access to the Schneider Electric customer care mobile application mySchneider app that can be downloaded on Android and iOS smartphones. For smartphone compatibility, check on your application store. The customer care application offers self-service instructions and easy access to expert support and information.

Schneider Electric Anti-Fake Query

Perform the following procedure to check anti-fake code:

  1. Scan the QR code.

    The following landing page of the contactor is displayed with the following information.

  2. Click More details.

    The following page is displayed.

  3. Click copy icon to copy the anti-fake code and click OK to return to the previous page.

  4. Click Schneider Electric Anti-Fake Query.

    The following page is displayed.

  5. Paste the anti-fake code in the Anti-fake code field.

  6. Enter your Customer Name and Mobile Number.

  7. Type the displayed verification code in the Verification code field.

  8. Click Check Now.

    The following page is displayed if the device is a genuine TeSys Giga device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.