DOCA0191EN–05

Removing the Conductor from the Terminal

  1. Loosen the screws to release the conductor from the terminal.
  2. Pull the conductor out from the terminal.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?