DOCA0191EN–05

Diagnosis LED

The below table provides the different LED indication functions:

LED indication

Diagnosis indication

Diagnosis function

The contacts are worn, see Diagnosis Functions

Diagnosis contact wear

The control voltage is lower than 80 % of Ucmin, and the contactor is open, see Diagnosis Functions

Under voltage

The control voltage is higher than 110 % of Ucmax, see Diagnosis Functions

Over voltage

The remote wear diagnosis module is not synchronized with the contactor, see Diagnosis Functions

Remote wear diagnosis module synchronization

The wear diagnosis reset is in progress, see Switching Module Replacement

Reset of remote wear diagnosis

A control module internal malfunction is detected, see Troubleshooting

Internal functioning

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?