TeSys Giga Contactor Assembly with TeSys Giga Overload Relay Separately Mounted
Overview
The mounting base is used for separately mounting of overload relay beneath contactor to align the power connections of the contactor and the overload relay, to allow connection between the contactor and the overload relay with straight bars.
|
Description |
Mounting base reference |
|---|---|
|
Mounting base for alignment of LR9G115-225C with LC1G205-245C |
LA9G3650 |
|
Mounting base for alignment of LR9G500C with LC1G300C |
LA9G3651 |
|
Mounting base for alignment of LR9G500C with LC1G410–475C |
LA9G3652 |
|
Mounting base for alignment of LR9G630C with LC1G620C |
LA9G3653 |