DOCA0191EN–05

Mounting Two-Contactor Changeover on Plate

Perform the following procedure to mount a two-contactor changeover with LA9G970 mechanical interlock on the plate.

  1. Drill 8 holes in the plate, with respect of the dimensions.

    • LC1G205-475C - Maximum hole diameter: 6 mm

    • LC1G620C - Maximum hole diameter: 9 mm

    NOTE: To ease the mounting, drilling stencils JYT1902701 can be downloaded from the www.se.com website.
     

    LC1G205-245C

    LC1G300-475C

    LC1G620C

    G

    35 mm

    45 mm

    70 mm

    J

    166 mm

    187 mm

    242 mm

    X

    92.7 mm

    115 mm

    160 mm

  2. Remove the plastic part on the side of the contactor where the mechanical interlock will be installed.

  3. Discard the plastic part into the bin.

  4. Insert the metal slides on the holes of each contactor.

  5. Mount each contactor on the plate.

  6. Assemble the mechanical interlock according to the rating of the contactors.

     

    LC1G205–245C

    LC1G300–475C

    LC1G620C

    -

    -

  7. Insert the mechanical interlock between the two contactors on the metal slides.

  8. Tighten the two screws at the right torque to lock the interlock.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?