DOCA0191EN–05

Current–Based Protection Functions

There are four current–based protection functions provided by the overload relay :

  • Thermal overload protection

  • Phase loss protection

  • Phase imbalance protection

  • Ground–fault protection

Operation

The state of the auxiliary contacts of the overload relay changes, when a protection function triggers a tripping:

  • NC 95/96 contact state changes from closed to open.

  • NO 97/98 contact state changes from open to closed.

The trip state is latched and is indicated by the trip indicator on the front face of the overload relay . A reset action is required to acknowledge the trip condition and to release the auxiliary contacts.

The auxiliary contacts of the overload relay can be used as follows:

  • the NC contact can be used to switch off the contactor and then stop the motor.

  • the NO contact can be used to signal remotely the state of the overload relay .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.