DOCA0191EN–05

Coding Principle

The commercial reference of Tesys Giga contactors is coded with significant features to explain the type of contactor, current ratings at 440 Vac for AC-3 utilization category and control voltage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?