DOCA0191EN–05

Modbus Register Tables

Table Formats

Register tables have the following columns:

Address

Register

Number of 16-bit registers

R/W

Type

Description

Designation

Description

Address

16-bit register address in hexadecimal. The address is the data used in the Modbus frame.

Register

16-bit register number in decimal. Register = Address + 1. For example, the register 60001 is addressed as 0xEA60.

Number of 16-bit registers

Number of 16-bit registers that need to be read / written to access the complete information.

R/W

Whether the register is read only (R) or read-write (RW).

Type

Coding data type (see Data Types table below).

Description

Information about the register and restrictions that apply.

Data Types

Name

Description

UINT16

16-bit unsigned integer (1 word)

UINT32

32-bit unsigned integer (2 word)

ASCII

String of 8–bit alphanumeric character

Register Table

Address

Register

Number of 16-bit registers

R/W

Type

Description

0xEA60

60001

9

R

ASCII

The vendor’s name of the product: Schneider Electric

0xEA69

60010

32

R

ASCII

The URL of the vendor: https://www.se.com/

0xEAC4

60101

8

R

ASCII

Product range name: TeSys Control

0xEADC

60125

8

R

ASCII

Product family name: Motor Starter

0xEB32

60211

1

R

UINT16

Internal numerical identifier of the product: 19800

0xEB33

60212

20

R

ASCII

Serial number of control module. A unique number of each control module delivered.

0xEF11

61202

1

R

UINT16

Status of the contactor:

0: Open

1: Close

0xEF75

61302

1

R

UINT16

Bitmap for diagnosis indication:

0: Inactive

1: Active

Bit definition:

bit 0: The remaining service life of contacts is below 15%

bit 4: Control voltage estimated value is over the maximum value of rated control voltage range

bit 5: Control voltage estimated value is under the minimum value of rated control voltage range

bit 7: Control module temperature is over the operation limit

Other bits: Reserved

0xEF76

61303

1

R

UINT16

Bitmap for internal malfunction indication:

0: Inactive

1: Active

Bit definition:

bit 1: EEPROM error

Other bits: Reserved

0xEFDD

61406

1

R

UINT16

The actual control voltage (V)

0xF03C

61501

2

R

UINT32

The number of operations performed by the contactor during its lifetime

0xF0A0

61601

2

R

UINT32

Event record 1 (latest record), see Event Records

0xF0A2

61603

2

R

UINT32

Event record 2, see Event Records

0xF0A4

61605

2

R

UINT32

Event record 3, see Event Records

0xF0A8

61609

2

R

UINT32

Event record 4, see Event Records

0xF0AA

61611

2

R

UINT32

Event record 5, see Event Records

0xF105

61702

1

R/W

UINT16

Digital output mapping for diagnosis indication

0: Disabled (default)

1: Enabled

Bit definition:

bit 0: The remaining service life of contacts is below 15%

bit 1: Control voltage estimated value is over the maximum value of rated control voltage range

bit 2: Control voltage estimated value is under the minimum value of rated control voltage range

bit 3: Control module temperature is over the operation limit

Other bits: Reserved (must be set to 0)

NOTE: The RDM module will answer with invalid data 0x8000 if an unused register is read. See Troubleshooting for more details.

Event Records

The RDM module records the last 5 encountered events. Event record 1 shows the latest event, and event record 5 shows the oldest event. Earlier event records are overwritten by new ones.

Each event record consists of two 16-bit registers:

Event index (UINT8)

Event type (UINT8)

Event data (UINT16)

  • Register 1 MSB: unique index of each event record. It increases with the occurrence of events, from 0x01 to 0xFF.

  • Register 1 LSB: type of events. See the following table.

  • Register 2: data related to the event. See the following table.

Type of the event

Data related to the event

Event description

0x01

0xFFFF (N/A)

Wear diagnostic alarm activated

0x02

Voltage RMS in V

Contactor over voltage detected

0x03

Voltage RMS in V

Contactor under voltage detected

0x04

0xFFFF (N/A)

Contactor over temperature detected

0xFF

0xFFFF (N/A)

No event. Default event for event record

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.