DOCA0191EN–05

Overview

TeSys Control-Giga contactors are high power contactors (up to 620 A AC-3 or 1050 A AC-1) for AC/DC motor applications and AC/DC load applications. They can be used up to 1000 Vac power voltage and up to 460 Vdc power voltage..

They are available with 3 main poles that have the same width and the same pole pitch as the associated Schneider Electric circuit breaker.

They can be supplied either by AC or DC control voltage and has the built-in surge suppressors. They can operate with a wide control voltage band. If they are supplied by DC control voltage, there is no need to respect the polarity.

They embed diagnosis functions as contact wear diagnosis or control voltage diagnosis. They are delivered with one auxiliary contact module of two auxiliary contacts (1NO+1NC) with screw terminals. The auxiliary NC contact mirrors the state of the main poles and the auxiliary NO contact is mechanically linked to the NC auxiliary contact.

The control module controls the contactor by A1-A2 terminals. They can operate with 48-130, 100-250 or 200-500 Vac/Vdc control voltage ranges. The A1-A2 terminals are removable and use screw technology.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?