DOCA0191EN–05

Straight Terminal Extensions

Overview

The straight terminal extensions are used to extend the connexion possibilities of the contactor.

The terminal extensions are screwed on the contactor using the screws delivered with the contactor.

The screws delivered with the terminal extensions are used to screw bars or lugs on the terminal extensions.

The table below provides the list of the straight terminal extensions:

Contactor

Straight terminal extension

LC1G205-245C

LA9G3601

LC1G300-475C

LA9G3602

LC1G620C

LA9G3603

Dimension

Contactor

W

H

D

LC1G205-245C

88 mm

34.5 mm

69.5 mm

LC1G300-475C

120 mm

36 mm

84 mm

LC1G620C

188 mm

49.7 mm

113 mm

For installation instructions of power connection accessories, see Installation of the Power Connection Accessories

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.