DOCA0191EN–05

Mounting LC1G205-245C Contactors on Plate

Perform the following procedure to mount the LC1G205-245C contactors on the plate.

  1. Drill 4 holes in the plate. Hole diameter: 4.5 to 6 mm .

  2. Insert the two short screws (A) diagonally on the plate and tighten the screws with PZ2 screwdriver at the right torque.

  3. Place the contactor on the short screw heads.

  4. Insert the two long screws (B) diagonally through the contactor and tighten them at the right torque.

Contactor

G

J

Screws

LC1G205-245C

35 mm

166 mm

M5

NOTE: The four screws with nuts and washers are delivered with contactors .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?