DOCA0191EN–05

Spreaders

Overview

The spreaders are used on contactors:

  • to increase the pole pitch of the contactor and align the contactor poles with circuit breaker poles or

  • to increase the clearance distance between phases or

  • to connect larger bars or lugs.

The spreaders are screwed on the contactor using the screws delivered with the contactor.

The screws delivered with the spreaders are used to screw bars or lugs on the spreaders.

The table below provides the list of spreaders used with contactors :

Contactor

Spreaders

LC1G205-245C

LA9G3611

LC1G300-475C

LA9G3612

Dimension

 Contactor

W

H0

H1

D

LC1G205-245C

108 mm

44 mm

54.5 mm

69.5 mm

LC1G300-475C

170 mm

61 mm

73 mm

84 mm

For installation instructions of power connection accessories, see Installation of the Power Connection Accessories.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.