DOCA0191EN–05

Overload Relay Wiring Characteristics

The table below provides wiring characteristics of the screw terminals blocks of overload relays:

Cable type

Stripping length

Number of conductors

Section

Solid Cable

10 mm

1 conductor without cable end

0.2–2.5 mm²

2 conductors without cable end

0.2–1 mm²

2 conductors with suitable dual sleeve

0.5-1.5 mm²

Flexible cable

1 conductor with suitable cable end or sleeve

0.25-2.5 mm²

2 conductors with suitable cable end

0.25-1 mm²

2 conductors with suitable dual sleeve

0.5-1.5 mm²

Do not use flexible cable without cable end or sleeve.

For the overload relay wiring diagram, see Wiring Diagram.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.