DOCA0191EN–05

Power Connection with Changeover Connection Kits

Overview

Changeover connection kits can be used for the power connection of two-contactor changeover. If using the connection kits, the two contactors must be fitted with a cable memory or must be without cable memory. This connection can be done only downstream of the contactors.

Changeover connection kits are made of one coupling bar.

The table below provides the list of the changeover connection kits:

Contactor

Changeover connection kits

LC1G205-245C

LA9G3750

LC1G300-475C

LA9G3751

LC1G620C

LA9G3752

Dimensions

Commercial reference

W0

W1

H0

D0

D1

LA9G3750

215.7 mm

232.6 mm

31.5 mm

23.6 mm

68.5 mm

LA9G4750

286 mm

303 mm

31.5 mm

23.6 mm

68.5 mm

LA9G3751

280 mm

298 mm

38 mm

79 mm

81 mm

LA9G4751

370 mm

388 mm

38 mm

79 mm

81 mm

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.