Loads per IEC Utilization Category
The table below indicates the loads compatible with the 3–pole contactors for IEC AC–1 utilization category .
|
3P contactors |
IEC AC-1 utilization category Maximum current (θ ≤ 40 °C) |
IEC AC-1 utilization category Maximum current (θ ≤ 60 °C) |
|
LC1G205●●●C LC1G205LSEMC |
305 A |
275 A |
|
LC1G245●●●C LC1G245LSEMC |
330 A |
300 A |
|
LC1G300●●●C LC1G300LSEMC |
440 A |
400 A |
|
LC1G410●●●C LC1G410LSEMC |
550 A |
500 A |
|
LC1G475●●●C LC1G475LSEMC |
700 A |
600 A |
|
LC1G620●●●C LC1G620LSEMC |
1050 A |
800 A |