Mounting LC1G300-620C Contactors on Plate
-
Drill 4 holes in the plate, with respect of the dimensions given.
-
LC1G300-475C - Maximum hole diameter: 6 mm.
-
LC1G620C - Maximum hole diameter: 9 mm.
-
-
Insert the two short screws (A) diagonally on the plate.
-
LC1G300-475C - The distance between the panel and screw head flat surface shall be between 6 and 14 mm.
-
LC1G620C - The distance between the panel and screw head flat surface shall be between 16 and 24 mm.
-
-
Place the contactor on the screw heads.
-
Tighten the two screws with PZ2 screwdriver at the right torque.
-
Insert the two long screws (B) diagonally through the contactor and tighten them at the right torque.
| Contactor |
G |
J |
Screws |
|---|---|---|---|
| LC1G300-475C |
45 mm |
187 mm |
M5 |
|
LC1G620C |
70 mm |
242 mm |
M8 |