DOCA0191EN–05

Timer to Control the Contactors

For the star-delta connection, RE17RMMWS Timer (TMR) can be used to control the contactor up to 250 V.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?