Overview
The contactor poles are designed as replaceable switching modules. The switching modules must be replaced when the contact wear diagnosis function has detected that the contacts are worn. When the contacts are worn, all switching modules must be replaced together.
The table below provides the commercial references of the switching modules:
|
Contactor |
Set of 3 switching modules for 3P contactor |
|---|---|
|
LC1G205-245C |
LA9G3QA |
|
LC1G300C |
LA9G3RA |
|
LC1G410-475C |
LA9G3SA |
|
LC1G620C |
LA9G3TA |