DOCA0191EN–05

Loads

The contactors are designed to switch AC or DC loads. The IEC 60947-4-1 standard defines the utilization categories for a contactor .

The table below provides the definition of the AC utilization categories:

Term

Definition

AC–1

Non–inductive or slightly inductive loads, resistance furnaces

AC–2

Slip–ring motors: starting, switching off

AC–3

Squirrel–cage motors: starting, switching off motors during running, reversing

AC–3e

Squirrel-cage motors with higher locked rotor current: starting, switching off motors during running, reversing

AC–4

Squirrel–cage motors: starting, plugging, inching

AC–5a

Switching of electric discharge lamp controls

AC–5b

Switching of incandescent lamps

AC–6a

Switching of transformers

AC–6b

Switching of capacitor banks

AC–7a

Slightly inductive loads in household appliances and similar applications

AC–7b

Motor–loads for household applications

AC–8a

Hermetic refrigerant compressor motor control with manual resetting of overload releases

AC–8b

Hermetic refrigerant compressor motor control with automatic resetting of overload releases

The table below provides the definition of the DC utilization categories:

Term

Definition

DC-1

Non-inductive or slightly inductive loads

DC-3

Shunt-motors: starting, plugging, inching, dynamic breaking of DC motors

DC-5

Series-motors: starting, plugging, inching, dynamic breaking of DC motors

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.