DOCA0191EN–05

Hardware Description

Labels

Description

A

Power connections

B

A1–A2 control module terminal

C

Diagnosis orange LED

D

1 NO + 1 NC auxiliary contacts

E

Marking flap cover

F

QR code

G

Clip-on marker holder

H

ON/OFF status indicator

I

Diagnosis reset switch

J

Remote diagnosis Modbus module plug

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?