DOCA0191EN–05

Identification with Clip-On Marker Holder

There is a clip-on marker holder on the front face of each contactor and overload relay. The dimension of the marker holder is 8 x 18 mm .
NOTE: Spare marker holder can be ordered with the commercial reference LA7D903 (set of 100 marker holders).

Perform the following procedure to identify an equipment with a marker holder.

  1. Unclip and remove the marker holder from contactor or overload relay.
  2. Write the identification code of the contactor or overload relay on the marker holder.
  3. Clip the marker holder back on contactor or overload relay.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?