DOCA0191EN–05

Removal of Contactor

Before replacing the switching modules on a contactor :
  • Remove the mechanical interlock and coupling bars, if present.

  • Remove all auxiliary contact modules.

  • Disconnect top and bottom power connections.

Perform the following procedure to remove the contactor :

  1. Unscrew the control terminal blocks.
  2. Remove the control terminal blocks.
  3. Disconnect the top and bottom power connections.
  4. Free the contactor from the power conductors.
  5. Unscrew with an Allen key the 4 screws fixing the contactor block in the contactor housing.
  6. Remove the contactor block from the contactor housing.

Contactor

Tool

Screws

LC1G205-245C

Allen key

M8

LC1G300-475C

Inner hexagon

M10

LC1G620C

Inner hexagon

M12

Contactor

Tool

Length of Allen Key (L)

Screws

LC1G205-245C

Allen key

≥ 95 mm

M4

LC1G300-475C

Allen key

≥ 115 mm

M4

LC1G620C

Allen key

≥ 115 mm

M6

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?