DOCA0191EN–05

Edgewise Terminal Extensions

Overview

The edgewise terminal extensions are used to extend the connexion possibilities of the contactor.

The terminal extensions are screwed on the contactor using the screws delivered with the contactor.

The screws delivered with the terminal extensions are used to screw bars or lugs on the terminal extensions.

The table below provides the list of the edgewise terminal extensions:

Contactor

Edgewise terminal extensions

LC1G205-245C

LA9G3631

LC1G300-475C

LA9G3632

LC1G620C

LA9G3633

Dimension

Contactor

W

H0

H1

D

LC1G205-245C

94 mm

27.5 mm

38.5 mm

59.5 mm

LC1G300-475C

120 mm

64.5 mm

78.5 mm

70 mm

LC1G620C

148 mm

93 mm

111 mm

93 mm

For installation instructions of power connection accessories, see Installation of the Power Connection Accessories.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.