DOCA0191EN–05

Weights

This section describes the weights for theTeSys Control-Giga contactors and TeSys Protect-Giga electronic overload relays .

Device

Commercial references

Weight

Contactor

LC1G205–245C

3.6 kg

LC1G300–475C

7.5 kg

LC1G620C

14 kg

Overload relay

LR9G115-225C

0.80 kg

LR9G500C

1.33 kg

LR9G630C

2.23 kg

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.