DOCA0191EN–05

Overview

Remote Diagnostic Modbus (RDM) module supports Modbus communication and one digital output (DO). It is used to provide diagnosis indications remotely for contactors with a control module with commercial references ending with LSEMC, including:

  • main contact wear diagnosis

  • coil over-temperature

  • coil over-voltage and under-voltage

  • control module internal malfunction

  • contactor operating times

It can record the latest five diagnosis events. See Diagnosis Functions.

The table below provides the compatibility of the RDM module with contactors and control modules:

Contactor

Control module

RDM module reference number

LC1G205-245LSEMC

LX1G3QLSEMC

LA9GRDMD

LC1G300LSEMC

LX1G3RLSEMC

LA9GRDMD

LC1G410-475LSEMC

LX1G3SLSEMC

LA9GRDMD

LC1G620LSEMC

LX1G3TLSEMC

LA9GRDMD

Hardware Description

Label

Description

A

Plug to the contactor

B

Unlock trigger

C

Terminal block for digital output, RDM power supply and Modbus communication port

D

LED indicator

E

Modbus address tens-digit knob

F

Modbus address ones-digit knob

G

Baud rate and parity setting knob

LED Indicator

LED status

Color

Indication

On

Green

Initial idle state after RDM module is powered on. No request received.

Orange

RDM module is powered on and a Modbus error is detected. See Troubleshooting for more details.

Red

RDM module is not powered and a Modbus error is detected. See Troubleshooting for more details.

Blinking

Green and orange

RDM module is powered on, and Modbus communication is ongoing without error.

If a Modbus exception code is returned, see Troubleshooting for more details.

Off

-

RDM module is powered off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.