DOCA0191EN–05

Motor ON and Alarm LEDs

LED

LED status

Indication

Motor ON

Green steady

The motor is supplied:

  • On LR9G115C or LR9G225C relays: the current measured is higher than 25 A

  • On LR9G500C or LR9G630C relays: the current measured is higher than 50 A

Green blinking

An overload relay internal malfunction is detected, see Troubleshooting

Alarm

Orange steady

Overload alarm: 90% of the motor thermal capacity is reached

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.