DOCA0191EN–05

Connection with Bars

Overview

Bars can be used to connect contactors and overload relays . These are provided by the installer. The bars can be installed both upstream and downstream of contactors and overload relays .

Dimensions

Contactor

Giga relay

A

B

C

Ø

LC1G205-245C

LR9G115-225C

≤ 25 mm

≤ 10 mm

≤ 6 mm

9 mm

LC1G300-475C

LR9G500C

≤ 32 mm

≤ 15 mm

3 mm ≤...≤ 10 mm

10.6 mm

LC1G620C

LR9G630C

≤ 50 mm

≤ 15 mm

3 mm ≤...≤ 10 mm

13 mm

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.