DOCA0191EN–05

Thermal Dissipation

This section describes the thermal dissipation characteristics for the contactors and control modules, and thermal overload relays.

Main Power Lines of Contactors

Contactor

Power dissipation per pole at maximum current with AC–1 load

Power dissipation per pole at maximum current with AC–3/AC–3e load

LC1G205C

20 W

6 W

LC1G245C

20 W

8 W

LC1G300C

30 W

16 W

LC1G410C

30 W

16 W

LC1G475C

40 W

20 W

LC1G620C

70 W

26 W

Contactors Control Modules

Contactor

Heat dissipation for control module

LC1G205–245C

5–6 W

LC1G300C

6–7 W

LC1G410–475C

6–7 W

LC1G620C

6–7 W

Overload Relays

Overload relay

Maximum heat dissipation at Ir Max

LR9G115C

1 W

LR9G225C

3 W

LR9G500C

5 W

LR9G630C

8 W

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.