DOCA0191EN–05

Bar or Lug Connection

  1. Place the bar or lug of the power circuit on the terminal extension.

  2. Connect the terminal extensions to the power circuit using the screws delivered with the terminal extensions.

  3. Tighten the screws at the right torque. The torques are the same as the torques to connect the terminal extensions on the contactor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?