DOCA0191EN–05

Physical Security of the Device

The following is the important physical security point to keep in mind for installing the device:

For Modbus-RTU accessories which are recognized as having security risks in the industry, physical security measures (such as dedicated pipes) are recommended to protect communication cables from unauthorized access, communication drops, data leakage and tampering, etc.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.