DOCA0191EN–05

Motor Ratings per IEC Utilization Categories

The table below indicates the motor ratings compatible with the 3–pole contactors for AC–3, AC–3e, and AC-4 utilization categories.

3P contactors

Category

230 Vac

400 Vac

415 Vac

440 Vac

500 Vac

690 Vac

1000 Vac

LC1G205●●●C

LC1G205LSEMC

AC-3

63 kW

110 kW

110 kW

110 kW

129 kW

129 kW

100 kW

AC-3e

63 kW

110 kW

110 kW

110 kW

129 kW

129 kW

100 kW

AC-4

55 kW

90 kW

90 kW

100 kW

110 kW

110 kW

75 kW

LC1G245●●●C

LC1G245LSEMC

AC-3

75 kW

132 kW

132 kW

132 kW

160 kW

160 kW

147 kW

AC-3e

75 kW

132 kW

132 kW

132 kW

160 kW

160 kW

147 kW

AC-4

55 kW

110 kW

110 kW

129 kW

132 kW

132 kW

110 kW

LC1G300●●●C

LC1G300LSEMC

AC-3

100 kW

160 kW

180 kW

195 kW

200kW

220 kW

160 kW

AC-3e

100 kW

160 kW

180 kW

185 kW

200kW

220 kW

160 kW

AC-4

90 kW

160 kW

160 kW

185 kW

200 kW

220 kW

185 kW

LC1G410●●●C

LC1G410LSEMC

AC-3

110 kW

220 kW

220 kW

250 kW

250 kW

280 kW

185 kW

AC-3e

110 kW

220 kW

220 kW

250 kW

250 kW

280 kW

185 kW

AC-4

110 kW

200 kW

200 kW

220 kW

250 kW

315 kW

220 kW

LC1G475●●●C

LC1G475LSEMC

AC-3

147 kW

265 kW

280 kW

280 kW

355 kW

335 kW

335kW

AC-3e

147 kW

265 kW

265 kW

280 kW

315 kW

335 kW

335kW

AC-4

150 kW

250 kW

250 kW

295 kW

295 kW

355 kW

280 kW

LC1G620●●●C

LC1G620LSEMC

AC-3

200 kW

335 kW

375 kW

400 kW

400 kW

450 kW

450 kW

AC-3e

180 kW

335 kW

335 kW

355 kW

400 kW

450 kW

450 kW

AC-4

180 kW

315 kW

335 kW

355 kW

375 kW

450 kW

355 kW

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?