Mounting Two-Contactor Reverser on Plate
Perform the following procedure to mount a two-contactor reverser with LA9G970 mechanical interlock on the plate.
-
Drill 8 holes in the plate, with respect of the dimensions given.
-
LC1G205-475C - Maximum hole diameter: 6 mm
-
LC1G620C - Maximum hole diameter: 9 mm
NOTE: To ease the mounting, drilling stencils JYT1902701 can be downloaded from the www.se.com website.LC1G205-245C
LC1G300-475C
LC1G620C
G
35 mm
45 mm
70 mm
J
166 mm
187 mm
242 mm
X
92.7 mm
115 mm
160 mm
-
-
Remove the plastic part on the side of the contactor where the mechanical interlock will be installed.
-
Discard the plastic part into the bin.
-
Insert the metal slides on the holes of each contactor.
-
Mount each contactor on the plate.
-
For mounting LC1G205-245C contactors, see Mounting LC1G205-245C Contactors on Plate
-
For mounting LC1G300-620C contactors, see Mounting LC1G300-620C Contactors on Plate
-
-
Assemble the mechanical interlock according to the rating of the contactors.
-
Insert the mechanical interlock between the two contactors on the metal slides.
-
Tighten the two screws at the right torque to lock the interlock.