DOCA0191EN–05

TeSys Giga Contactor Mounting on Plate

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Install the contactor so that the minimum clearance to grounded metal is maintained.
Failure to follow these instructions will result in death or serious injury.

The contactor can be mounted

  • either on a plate drilled with simple holes, using the screws, washers and nuts delivered with the contactors

  • or on a plate drilled with threaded holes, using only screws adapted to the threaded holes.

NOTE: It is recommended to use a steel plate with minimum thickness of 2 mm.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.