DOCA0191EN–05

Ir/FLA Setting

The Ir/FLA setting corresponds to the rated current of the motor or full load amp and can be adjusted with a 64-position rotary switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?