AU Execution Options Table

This table must be named SE_AU_EXEC_OPTIONS__. The table’s function is to pass autoupdater execution options from a client by serializing them into the OPTIONS field of the table.

The table’s fields are displayed below:


Field

Alias

Type

Notes

OBJECTID

OBJECTID

OID

 

GlobalID

GlobalID

GlobalID

 

created_user

created_user

String

 

created_date

created_date

Date

 

last_edited_user

last_edited_user

String

 

last_edited_date

last_edited_date

Date

 

OPTIONS

OPTIONS

BLOB

 

The format of the data serialized in the OPTIONS field is composed of the properties below:

Property

Description

Example Value

skipAll

A boolean indicating whether to skip execution of all autoupdaters.

Default value is false.

true

ignoreOptionsTableEdits

A boolean indicating whether to ignore edits to the AU Execution Options table.

Default value is true.

Setting this to false in the client will allow for an autoupdater to modify data in the AU Execution Options table, effectively creating two-way communication between that client and an autoupdater. As a consequence, the client is required to maintain the rows that may end up being created in the table.

false

propertyBag

A property bag containing custom data. The keys are of type string and the values are of type JObject (see JObject Class).

{       
"customProp1": "Value1",
"customProp2": 123
}

When all the property values are written into the field, it may look something like the example below:

{    
	"skipAll": true,
	"ignoreOptionsTableEdits": false,
	"propertyBag":
	{       
		"customProp1": "Value1",
		"customProp2": 123
	}
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.