DOCA0172EN-15

Hardware version

The following models of EcoStruxure Panel Server are released with hardware version 002.000.000 (HW: V02):

  • PAS600P

  • PAS600PWD

  • PAS600LWD

Certain models of Universal and Advanced EcoStruxure Panel Server exist in two hardware versions: 001.000.000 and 002.000.000 (HW: V02). Both versions offer the same capabilities and functionality. For PAS600 and PAS600L, hardware version 002.000.000 allows you to add an external IEEE 802.15.4 antenna, not available for hardware version 001.000.000.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?