DOCA0172EN-20

EcoStruxure Panel Server System

Architecture

From a simple electrical distribution system with one device to large electrical distribution systems, the EcoStruxure Panel Server collects data from any of the supported devices.

The following illustration shows typical architectures of EcoStruxure Panel Server:

Ethernet or Wi-Fi LAN
Modbus-SL communication
ULP system
Digital inputs/outputs
IEEE 802.15.4 wireless communication
Wi-Fi access point

Network Connectivity

EcoStruxure Panel Server network connectivity can be subdivided into two parts:

  • Upstream connection to supervision software and cloud applications.

  • Downstream connection to local field devices.

Upstream Connection

The upstream network of EcoStruxure Panel Server can be used to connect cloud applications or Modbus TCP/IP monitoring and supervision application.

  • Entry model:

    This access is provided either through the Ethernet port on the Panel Server or through the Wi-Fi interface.

  • Universal and Advanced models:

    This access is provided through the two Ethernet ports on the EcoStruxure Panel Server or through the Wi-Fi interface, where applicable.

    Depending on the Ethernet port configuration, the data transmission behavior is as follows:

    • In switched mode (default mode), the two Ethernet ports are connected to the internal Ethernet switch of the EcoStruxure Panel Server. Devices connected to either of the Ethernet ports can see each other.

    • In separated mode, Ethernet port ETH1 is connected to the upstream network while Ethernet port ETH2 is used to create a downstream Ethernet network separate from the upstream Ethernet network.

    In case of Wi-Fi connection, Wi-Fi is always considered the upstream network and the Ethernet ports are separated from the Wi-Fi network. The upstream (Wi-Fi) network and downstream (Ethernet) network(s) must be different networks using different subnets (see following table. In the table A, B and C represent different networks.):

    Connection Wi-Fi network ETH1 network ETH 2 network

    Switched mode (Wi-Fi not activated)

    A

    A

    Separated mode (Wi-Fi not activated)

    A (upstream)

    B (downstream)

    Wi-Fi and switched mode

    A (upstream)

    B (downstream)

    B (downstream)

    Wi-Fi and separated mode

    A (upstream)

    B (downstream)

    C (downstream)

Downstream Connection (Entry Model)

Devices in the downstream network can be connected to the Panel Server Entry wireless concentrator through wireless network according to IEEE 802.15.4.

Downstream Connection (Universal and Advanced Models)

Devices in the downstream network can be connected to Panel Server Universal and Advanced through different means:

  • Wireless network according to IEEE 802.15.4 (PAS600, PAS600T, PAS600L, and PAS800 series)

  • Modbus-SL

  • Modbus TCP/IP (Ethernet and Wi-Fi)

  • Panel Server digital inputs (PAS600L, PAS600LWD, PAS800L)

Depending on the configuration of the Panel Server Ethernet ports, data transmission behavior is as follows:

  • In switched mode, it is possible to daisy chain several network devices via the Panel Server. The Modbus TCP/IP devices connected to either port of the Panel Server can be directly accessed by monitoring and supervision software running on a device physically connected to either ETH1 or ETH2 port.

  • In separated mode, the Modbus TCP/IP devices connected via the ETH2 port to the downstream Ethernet network may be accessed by upstream monitoring and supervision software through ETH1 port.

Supported Devices

List of supported devices (depending on Panel Server model):

  • Wired devices communicating through Modbus-SL, Modbus TCP/IP, or digital inputs:

    • Circuit breakers and switch-disconnectors

    • Protection relays

    • Power meters

    • Energy meters

    • Pulse meters

    • IO modules

    • Gateways

  • Wireless devices:

    • Energy-related devices:

      • PowerTag Energy and PowerLogic Tag power meters

      • Acti9 Active

    • Environmental sensors:

      • PowerLogic TH110/CL110

      • HeatTag sensors

      • Wireless CO2 sensors

      • Wireless temperature and humidity sensors

      • PowerTag Ambient

      • PowerLogic Thermal Tag TH150/TH200 wireless temperature sensors

    • Control devices:

      • PowerTag Control

      • Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

    • Circuit breakers: MicroLogic Active AP or EP control unit in MasterPacT MTZ circuit breakers

    • Other wireless devices:

      • PowerLogic PD100

      • Exiway Link emergency lighting devices

      • XB5R transmitters (ZBRT)

The devices supported by the Panel Server are listed in the respective release notes:

  • DOCA0249•• EcoStruxure Panel Server Entry - Firmware Release Notes

  • DOCA0178•• EcoStruxure Panel Server Universal - Firmware Release Notes

  • DOCA0248•• EcoStruxure Panel Server Advanced - Firmware Release Notes

Panel Server Entry Maximum Configuration

The table shows the maximum number of devices that can be configured in a system with a Panel Server Entry.

Wireless device

Maximum number of concurrent devices

PowerTag Energy sensors

20

PowerLogic Tag energy sensors

20

Acti9 Active devices

20

PowerTag Control devices

10

Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

20

MasterPacT MTZ circuit breakers with MicroLogic Active AP or EP control unit

8

Wireless CO2 sensors

20

Wireless temperature and humidity sensors

20

PowerTag Ambient sensors

20

PowerLogic TH110/CL110 environmental sensors

20

PowerLogic Thermal Tag TH150/TH200 wireless temperature sensors

20

PowerLogic HeatTag sensors

15

PowerLogic PD100 devices

15

Exiway Link devices

20

XB5R transmitters (ZBRT)

20

The recommendation for a mixed configuration of wireless devices is that any combination of wireless devices listed in the rows above should not exceed 20 devices.

For more information, contact your local Schneider Electric representative.

Panel Server Universal and Advanced Maximum Configuration

The maximum number of devices that can be configured in a system with a Panel Server Universal or Advanced depends on the type of connected devices:

Device type

Maximum number of concurrent devices

Wireless device (not supported by PAS600LWD and PAS600PWD)

PowerTag Energy sensors

85

PowerLogic Tag energy sensors

85

Acti9 Active devices

85

Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

85

MasterPacT MTZ circuit breakers with MicroLogic Active AP or EP control unit

8

Wireless CO2 sensors

100

Wireless temperature and humidity sensors

100

PowerTag Ambient sensors

100

PowerLogic TH110/CL110 environmental sensors

100

PowerLogic Thermal Tag TH150/TH200 wireless temperature sensors

100

PowerLogic HeatTag sensors

15

PowerTag Control devices

10

PowerLogic PD100 devices

15

Exiway Link devices

20

XB5R transmitters (ZBRT)

100

The recommendation for a mixed configuration of wireless devices is as follows:

  • Any combination of wireless devices listed in the rows above should not exceed 40 devices.

  • The total number of PowerTag Control, PowerLogic HeatTag, PowerLogic PD100, MicroLogic Active AP or EP control unit for MasterPacT MTZ, and Exiway Link devices should not exceed 20 devices.

Modbus-SL devices

Modbus-SL devices other than I/O devices:

32

NOTE: The maximum number depends on the serial line length and the type of device(s).

I/O devices:

  • I/O Smart Link device

  • Acti9 Smartlink Modbus-SL device

  • SmartLink SIB gateway

  • 8 I/O Smart Link or Acti9 Smartlink Modbus-SL devices connected to Panel Server serial line

  • OR

    1 SmartLink SIB + 7 I/O Smart Link or Acti9 Smartlink Modbus-SL devices

  • OR

    8 SmartLink SIB

Modbus TCP/IP devices

Devices physically connected to the Panel Server and virtual devices, that is, IEEE 802.15.4 wireless devices connected to a child Panel Server gateway.

128

NOTE: The Panel Server supports 64 simultaneous Modbus TCP/IP client connections (for example, SCADA system).

For more information, contact your local Schneider Electric representative.

Recommendations for Maximizing Performance (Panel Server Universal and Advanced)

  • Do not exceed the maximum number of Modbus-SL devices shown in the table above.

  • The suggested maximum of 32 Modbus-SL devices presumes a sampling period of 1 minute or more. Performance may be affected if lower sampling periods are used.

  • When the Panel Server is used as a transparent gateway, do not leave the devices connected to the Panel Server after testing or maintenance. Refer to Modbus Transparent Gateway.

  • For architectures including a SCADA system, connect a maximum of 8 Modbus-SL devices.

  • For architectures using Power Monitoring Expert, use the PME 2020 Daisy Chain Calculator to calculate the maximum configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.