DOCA0172EN-20

Monitoring and Control Menu

Overview

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not rely only on the measurements or equipment status provided on the Panel Server webpages before working on or inside the equipment.
Failure to follow these instructions will result in death or serious injury.

The webpage for the Monitoring and Control menu displays devices installed in the system and associated with the Panel Server.

Two views are available:

  • Device view: displays associated devices in a list in the left pane (tree view). The list can be displayed sorted by usage or by zone. Select the means to group the devices in the list by clicking the list icon . The device tree view can be collapsed. Monitoring and control data for the selected device is displayed in widgets in the main screen, with one widget for each data type.

    Global commands are available from Device view.

  • Multi-device view: Displays data from selected devices and up to two data types, as a table.

The data is refreshed automatically every 15 seconds in both views.

Device View

Click on a device name to see information specific to that device:

  • Header: Information about the device:

    • Device model

    • Device firmware version

    • Device serial number

    • Contextual data (if assigned):

      • Commodity

      • Usage

      • Zone

    • Device connection status

    • RF-ID of the device (wireless devices)

  • Data tab: Real-time data of the device, displayed as widgets, with one widget for each data type relevant to the device.

    The data is displayed as a graph or data values, depending on the data type.

    Active alarms are displayed when the following conditions are met:

    • the alarm is active when you access the webpages,

    • the alarm is not acknowledged.

    Control operations are displayed in the relevant widget as buttons which can be clicked to launch the operation.

  • Advanced data tab

The following individual commands can be sent from the Device view, depending on the device:

  • Reset all energies

  • Reset active power delivered - received peak demands

  • Breaker status position indicator status (Open/Closed)

  • Standard output disconnected off status (Off/Disconnected)

Icons at the top right of the page give you direct access to the following pages for that device:

  • Access to the device maintenance page by clicking the Maintenance icon .

  • Access to the device settings page by clicking the Settings icon .

  • Access to the data management page by clicking the Database icon .

  • Access to the trending data by clicking the Trending icon .

Multi-Device View

Select up to five devices and two data types from the drop down menus and click away from the list to display the results in a table. Select the means to group the devices in the list by clicking the list icon . The list is sorted in alphabetical order by Usage or by Zone.

The table displays:

  • A column with data and measurement names

  • A column for each selected device

  • A data block for Overview and each data type selected. The Overview block displays:

    • Label

    • Device family

    • Commodity

    • Usage

    • Zone

The following blocks display the data types selected. Empty cells indicate that no data is available for that device and data type.

Advanced Data

In the Monitoring and Control menu in Device view, the Advanced data tab of the selected device shows the exhaustive list of real-time data related to this device. The data is refreshed every 15 seconds.

The following table presents data available per measurement family. The availability of measurements depends on the type of connected device.

Data type

Data on Panel Server webpage

Active power

Active power total

Active power A

Active power B

Active power C

Power factor total

Apparent power

Apparent power total

Apparent power A

Apparent power B

Apparent power C

Circuit breaker

Breaker position

Trip indicator (SD position)

Trip cnt (Close to SD position) non resettable

Trip Electrical fault cnt (Close > SDE) non resettable

Current

Current

Current A

Current B

Current C

Current N

Current ground

Current THD

THD fund current A

THD fund current B

THD fund current C

THD fund current N

Embedded inputs

Status input 1

Status input 2

Consumption

Flow

Status output

Energy

Active energy delivered

Active energy received

Reactive energy delivered

Reactive energy received

Apparent energy

Apparent energy delivered

Environment

Temperature

Relative humidity

CO2 concentration

Air quality

Temperature phase A

Temperature phase B

Temperature phase C

Temperature neutral

Health state

Battery voltage

Internal temperature

RSSI link

Harmonic current

Load harmonics current A

Output harmonics current A

Load harmonics current B

Output harmonics current B

Load harmonics current C

Output harmonics current C

Output harmonics neutral current

IGBT temperature

Temperature board in device

Temperature IGBT A

Temperature IGBT B

Temperature IGBT C

Insulation

Insulation ground

Earth coupling capacity

Motor

Trip indicator

Motor running

Motor operating mode

Pole state

Contactor state

Speed setpoint

Motor speed

Direction of motor rotation

Reactive power

Reactive power total

Reactive power A

Reactive power B

Reactive power C

Unbalance

Current unbalance A

Current unbalance B

Current unbalance C

Current unbalance N

Voltage unbalance A-B

Voltage unbalance B-C

Voltage unbalance C-A

Voltage unbalance A-N

Voltage unbalance B-N

Voltage unbalance C-N

Voltage

Voltage L-L

Voltage A-B

Voltage B-C

Voltage C-A

Voltage L-N

Voltage A-N

Voltage B-N

Voltage C-N

Winding temperature

Temperature transformer winding A

Temperature transformer winding B

Temperature transformer winding C

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.